SparkFun Optoelektronika

Výsledky: 56
Zvolit Obrázek Č. dílu Výr. Popis Technické informace Dostupnost Stanovení ceny (CZK) Filtrovat výsledky v tabulce podle jednotkové ceny na základě zvoleného množství. Množství RoHS
SparkFun Světelné lišty a světlovody LED The WS2812 (often referred to as a "NeoPixel") has become the standard for addressable LED projects and development board indicator lights. While it may look like a common 5050-sized (5mm x 5mm) SMD LED it's far more advanced. Housed inside the tiny 14Na skladě
Minimum: 1
Vícenásobek: 1
SparkFun Vývojové nástroje optických snímačů The PureThermal 3 FLIR Lepton Smart I/O Module is a hackable thermal webcam module for the FLIR Lepton Longwave Infrared (LWIR) camera core. It ships preconfigured to operate as a plug-and-play UVC 1.0 USB thermal webcam that will work with standard 76Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Fotodiody The BPW34 is a tiny general purpose PiN photodiode. This photodiode has a ton of uses one of which is to use it is a mini solar cell to power your project. The cell is sensitive to a wide range of light wavelengths (430-1100nm) so it should produc 29Na skladě
Minimum: 1
Vícenásobek: 1
SparkFun Nástroje pro vývoj osvětlení LED Do not look into the light. You know you want to but boy will you be sorry. 1W per channel RGB High Power LEDs in one aluminum backed package. These LEDs will blow you away. Light them up then put a coffee cup over the LED to keep your eyes from se 21Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Vícebarevné LED Ever hear of a thing called RGB? Red Green Blue? How about an RGB LED? These 5mm units have four pins - one for each color and a common cathode (the longest pin). Use this LED for three status indicators or pulse width modulate all three and get mi 180Na skladě
Minimum: 1
Vícenásobek: 1
SparkFun Vývojové nástroje optických snímačů A simple breakout PCB for the GP1A57HR photo interrupter (also known as a photogate photodiode or phototransistor). This PCB has three connections for PWR GND and Signal.When the gate is clear SIG will be high (>4.9V). When the gate is blocked b 429Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Čočky fotoaparátu This is the 6mm CS-mount wide angle lens from CGL Electronics Co. Ltd. for use with the Raspberry Pi HQ Camera Module. The lens produces a 3MP picture in a 0.5in image format and is easily interchangeable using the thumb screw and adapter included wi 2Na skladě
Minimum: 1
Vícenásobek: 1
Ne
SparkFun Fotoaparáty a foto moduly The FLiR Dev Kit includes a breakout as well as a Lepton longwave infrared (LWIR) imager. With this kit you will be able to bring FLiR's thermal imaging reliability and power to your Arduino Raspberry Pi or any ARM based development tool all in a 3Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Displeje OLED a doplňky The SparkFun Qwiic OLED Display can display up to four lines of text and features 128x32 pixels in a compact 0.91-inch display. (diagonal) frame. As an OLED this display does not have a backlight layer (unlike LCDs); therefore it s thinner consu 114Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Fotoaparáty a foto moduly A first for the Raspberry Pi ecosystem: A 64MP camera module that matches the specs of smartphone cameras. The Arducam 64MP Camera Module puts a 64MP sensor with autofocus in the standard Raspberry Pi camera module form factor. Much like the other ca 7Na skladě
Minimum: 1
Vícenásobek: 1
SparkFun Vývojové nástroje optických snímačů Built around the STHS34PF80 sensor from STMicroelectronics this board is designed to give engineers the ability to easily experiment and develop applications with the sensor. The board measures 1" x 1" and includes two Qwiic sensors four mounting h 40Na skladě
Minimum: 1
Vícenásobek: 1
SparkFun Vývojové nástroje optických snímačů The SparkFun Qwiic Tristimulus Color Sensor is built around the OPT4048 High-Speed High-Precision Tristimulus XYZ Color Sensor from Texas Instruments. This Sensor features a single-chip high-resolution color sensor capable of measuring four channels 13Na skladě
Minimum: 1
Vícenásobek: 1
SparkFun Vývojové nástroje optických snímačů The SparkFun Qwiic Mini Human Presence and Motion Sensor is built around the STHS34PF80 Low-power high-sensitivity infrared (IR) sensor for presence and motion detection from STMicroelectronics. This sensor features an infrared motion and presence d 29Na skladě
Minimum: 1
Vícenásobek: 1
SparkFun Nástroje pro vývoj osvětlení LED The PicoBuck LED Driver is an economical and easy to use driver that will allow you to control and blend three different LEDs on three different channels. By default each channel is driven at 330mA; that current can be reduced by either presenting a 113Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Nástroje pro vývoj osvětlení LED This is the FemtoBuck a small-size single-output constant current LED driver. Each FemtoBuck has the capability to dim a single high-power channel of LEDs from 0-350mA at up to 36V while the dimming control can be either accessed via PWM or analog s 214Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Termokamery The PureThermal Mini Pro JST-SR is a powerful hackable thermal camera development kit designed for the FLIR Lepton thermal imaging core. This board combines plug-and-play simplicity with the advanced embeddable features that developers need. This k 5Na skladě
10Očekávané 28.05.2026 .
Minimum: 1
Vícenásobek: 1
SparkFun Vývojové nástroje optických snímačů SparkFun Spectr Sens Breakout AS7263 NIR 9Na skladě
53Očekávané 14.08.2026 .
Minimum: 1
Vícenásobek: 1

SparkFun Vývojové nástroje optických snímačů Ambient Light Sensor B/O TEMT6000 72Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Nástroje pro vývoj osvětlení LED The SparkFun Qwiic LED Stick features ten addressable APA102 LEDs making it easy to add full color LED control using I2C. Write to individual LEDs to display a count in binary or write to the whole strip for cool lighting effects. You can even add 68Na skladě
Minimum: 1
Vícenásobek: 1
SparkFun Displeje LED a příslušenství We are quite familiar with seven-segment displays. We see them on our alarm clocks ovens and microwaves. By adding more segments to each digit you can display more than just numbers! These green 14-segment displays allow you to show off all sorts o 10Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Displeje LED a příslušenství We are quite familiar with seven-segment displays. We see them on our alarm clocks ovens and microwaves. By adding more segments to each digit you can display more than just numbers! These 14-segment displays allow you to show off all sorts of numb 7Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Displeje LED a příslušenství We are quite familiar with seven-segment displays. We see them on our alarm clocks ovens and microwaves. By adding more segments to each digit you can display more than just numbers! These pink 14-segment displays allow you to show off all sorts of 7Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Displeje LED a příslušenství We are quite familiar with seven-segment displays. We see them on our alarm clocks ovens and microwaves. By adding more segments to each digit you can display more than just numbers! These red 14-segment displays allow you to show off all sorts of 8Na skladě
Minimum: 1
Vícenásobek: 1

SparkFun Vývojové nástroje optických snímačů This version of the QRE1113 breakout board features a digital output using a capacitor discharge circuit to measure the amount of reflection. This tiny board is perfect for line sensing when only digital I/O is available and can be used in both 3.3 19Na skladě
25Očekávané 09.06.2026 .
Minimum: 1
Vícenásobek: 1

SparkFun Vývojové nástroje optických snímačů RGB Light Sensor - ISL29125 39Na skladě
Minimum: 1
Vícenásobek: 1