PWM Controllers for Forward DC/DC Converters
Pulse Width
Modulation
(PWM) is widely used in switch mode power supplies that use digital control to provide the
switching
action. PWM itself is a controlled digital output signal. The PWM controller controls the rapid
switching in a power supply by sending a pulse to the gate driver that drives a power MOSFET (or
other switching device like a bipolar transistor, IGBT, etc.) One advantage of PWM is that the
signal is digital. Digital signals are more immune to noise, because a digital signal is either
a
binary “1” or “0.” Therefore noise can only change a digital signal if it is big enough to
change a
logical “0” to register at the receiving end as a logical “1”, or vice versa.
MOSFETs for Forward DC/DC Converters
Metal-oxide-semiconductor field-effect transistors (MOSFETs)
are
by far the most common of transistors today, being used for flash memory, processors,
random-access
memory (RAM), and application-specific integrated circuits (ASICs), and more. MOSFETs can be
conceptualized as a voltage-controlled device for limiting current flow.
MOSFETs are also for power switching circuits. Unlike bipolar junction transistors (BJTs), the
competing type of power transistor, MOSFETs do not require a continuous flow of drive current to
remain in the ON state. Additionally, MOSFETs can offer higher switching speeds, lower switching
power losses, lower on-resistances, and reduced susceptibility to thermal runaway. In
switched-mode
power supplies (SMPSs), MOSFETS are often used as the switching elements as well as for power
factor
correction (PFC).
Diodes for Forward DC/DC Converters
The first silicon-based
electronic component, diodes are passive devices which are found in virtually
every
electronic product or device. The ideal diode allows current to flow freely in one direction and
completely prevents current from flowing in the opposite direction. Although, at their core,
semiconductor diodes consist of a single P-N junction, there is vast array of different diode
types
and designs. The zener diode, for example, is designed to also conduct current in the opposite
direction when reverse-biased at or above a specific voltage threshold known as the "breakdown
voltage". AC/DC power supplies often employ diodes in a bridge-type configuration to rectify the
AC
input.
Capacitors for Forward DC/DC Converters
A
capacitor is a passive electronic component that stores energy in the form of
an
electric field. As part of an electrical circuit, capacitors "oppose" changes in voltage by
supplying (or drawing) current. An ideal capacitor is characterized simply by its capacitance
value,
the device's ability to store charge. However, a real-world capacitor has many additional
characteristics, such as tolerance rating, working voltage, leakage current, temperature
coeffecient, and equivalent series resistance (ESR) – each of which may carry a different level
of
importance for any given application.
Many types of capacitors exist to perform a variety of functions for a variety of different
applications. Decoupling capacitors protect electrical circuits from destructive voltage spikes
and
transients. Similarly, coupling capacitors serve to block direct current, which can cause damage
to
certain electronics, while only allowing the AC signal to pass. AC-to-DC power supplies use a
reservoir capacitor to smooth the output of a rectifier stage.
Inductors for Forward DC/DC Converters
Like a capacitor,
inductors are also passive energy-storing devices. Inductors, however, store
energy
in a magnetic field, and have the effect of opposing changes in current flow. An ideal inductor
is
characterized by a single value called inductance, which is measured in units called henries.
Physical, real-world inductors generally consist of a coil of wire wrapped around a core of
ferromagnetic material. However, not all inductors use a magnetic core, and the material used
directly affects the non-ideal properties of the device such as eddy current losses, magnetic
saturation, peak current, and high-frequency losses. Mutual inductance, formed by one or more
inductors with coupled magnetic flux, is the principle that underlies another electronic device,
the
transformer. In a switched-mode power supply, one or more inductors can be used for both output
filtering and energy storage (often implemented as a transformer).